AXIS#.GEAR.OUT

Description

This parameter is the numerator of the gear ratio for the electronic gearing mode. The gear ratio is used to increase/decrease the slave velocity. The slave velocity can be calculated by the following formula:

Slave velocity = Master velocity * AXIS#.GEAR.OUT/AXIS#.GEAR.IN

Be sure the external master source number of signals per revolution is set correctly. See AXIS#.GEAR.FBSOURCE to determine the gearing master source and verify the feedback resolution for that device.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

-32,768 to +32,767

Default Value

1

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.GEAR.OUT

5006h

04h

Signed16

-

-

Read/Write

No

AXIS2.GEAR.OUT

5106h

04h

Signed16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.GEAR.OUT

5504

1580

Signed16

Read/Write

-

AXIS2.GEAR.OUT

71040

1158

Signed16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.GEAR.OUT

5504

Signed16

Read/Write

-